Capital™ Capital HarnessXC: 线束映射关系被锁定且无法修改是什么原因?EN: Within Harness Mapping -> Target Harness Design, one target harness is locked and can't be changed, Why?

2023-09-20T01:35:04.000-0400
Capital Capital Harness Designer Capital Harness Designer Modular

摘要

在生成列表里一个线束的生成列表设置了两个目标线束,但现在想在映射里修改成另一个目标线束就不能更改,源线束和目标线束锁定。 EN: In HarnessXC -> Within Harness Mapping Dialog -> Target Harness Design, one target harness is locked and can't be changed, Why?


详细信息

在线束同步过程中,源数据来自上游工具比如Capital Logic或者Capital Topology或者Capital Integrator,目标线束设计创建于于Capital Harness XC中。
一般情况下,Capital Logic中的导线,连接器或者其它线束相关的对象会被赋予一个“线束属性”,这个线束属性可以用来匹配相同名称的线束设计,从而实现自动映射。
还有另外一种映射机制,即通过在目标线束设计上使用“线束组”来强制一个线束设计与源数据进行映射,并且这个映射关系一旦形成,用户是无法在“线束映射”对话框中进行修改。

Harness-Group-Definition

此时,如果想要把源数据映射到另一个线束设计,只需要把之前的线束设计上赋予的“线束组”给删除即可。然后就可以在线束映射对话框中重新选择目标线束。

EN:

Use of Harness Groups allows automapping of valid objects when Synchronizing from a Capital Logic Build List, where Capital Logic  objects need to be in multiple harnesses.

in HarnessXC tool, select the harness design and RMB then choose Edit Harness Design. A Harness Group name is specified for a design in this field. The same Harness Group name can be used on other designs. You must add this Harness Group name to the Harness attribute of the required objects in Capital Logic. Auto mapping matches these Harness Group names and synchronizes the Capital Logic object to all Harness designs with the same Harness Group tag. 

Harness Group names can be manually added here or, to select multiple Harness Groups, click the ellipsis (...) button to the right of the field to launch the Name Selection Dialog Box, from where you can select  predefined names. (Harness Group names are created and maintained in Capital Project, Object Type Information).​

 

Solution:

Delete the defined "Harness Group", then re-open the Harness Mapping dialog, then customer can freely select the target harness design.
Capital-HarnessXC-HarnessGroup

知识库文章 ID# KB000122282_ZH_CN

内容

摘要详细信息

关联组件

Capital HarnessXC Capital ModularXC