在生成列表里一个线束的生成列表设置了两个目标线束,但现在想在映射里修改成另一个目标线束就不能更改,源线束和目标线束锁定。 EN: In HarnessXC -> Within Harness Mapping Dialog -> Target Harness Design, one target harness is locked and can't be changed, Why?
Use of Harness Groups allows automapping of valid objects when Synchronizing from a Capital Logic Build List, where Capital Logic objects need to be in multiple harnesses.
in HarnessXC tool, select the harness design and RMB then choose Edit Harness Design. A Harness Group name is specified for a design in this field. The same Harness Group name can be used on other designs. You must add this Harness Group name to the Harness attribute of the required objects in Capital Logic. Auto mapping matches these Harness Group names and synchronizes the Capital Logic object to all Harness designs with the same Harness Group tag.
Harness Group names can be manually added here or, to select multiple Harness Groups, click the ellipsis (...) button to the right of the field to launch the Name Selection Dialog Box, from where you can select predefined names. (Harness Group names are created and maintained in Capital Project, Object Type Information).
Solution:
Delete the defined "Harness Group", then re-open the Harness Mapping dialog, then customer can freely select the target harness design.