Simcenter STAR-CCM+ Read-only Mode: 模拟文件的只读模式功能展示

2023-01-18T07:08:24.000-0500
Simcenter STAR-CCM+ Simcenter STAR-CCM+ Virtual Reality Teamcenter Share Simcenter STAR-CCM+ Viewer Simcenter STAR-CCM+ Application Specific Solutions

摘要

STAR-CCM+ 2021.1 (16.02) 发行模拟文件的只读模式 (Read-only Mode)新功能。它有3种场景应用,首先是阅读模型设定,其次模型文件对比,最后是加速与正确新模型文件设定。对于STAR-CCM+ Power session License 使用者需要在命令行加入命令,才能使用此功能。本案例将以STAR-CCM+ Power session License为演示对象。


详细信息

  1. 背景:
首先在License 选择 Read-Only Mode Fig 1所示,开启结果有报错信息如Fig 2Ask for 1 License of ccmpsuite
Graphical user interface, text, application, email  Description automatically generated
                                                          Fig 1
Graphical user interface, text, application, email  Description automatically generated
                                                                   Fig 2
 
  1. Solution
由于本案例是使用STAR-CCM+ Power session License,需要在Command 加入 “-power” (Fig 3)。执行结果如Fig 4,可以执行Read-only model功能。
Graphical user interface, text, application, email  Description automatically generated
                                                             Fig 3
Graphical user interface, text, application  Description automatically generated
                                                                  Fig 4

接下来本报告演示只读模式 (Read-only Mode)功能,3种场景应用。


(1) 阅读模型设定,在不会占用既有License数量下,可以浏览设定;如Fig 5所示查阅模型材料属性的密度设定。在查阅过程对于此模型不会发生被更改保存的风险出现。
Graphical user interface, text, application  Description automatically generated
                                                                                            Fig 5
(2) 模型文件对比,同时开启只读模式两个档案(Fig 6),选择File/ Comapre with (Fig 7),比对两个模拟文件,差异处使用粉红色着色(Fig 8)Graphical user interface, application  Description automatically generated
                                                                                           Fig 6
Graphical user interface  Description automatically generated
                                                                                                    Fig 7
Table  Description automatically generated
                                                                                                                    Fig 8
(3) 加速与正确新模型文件设定: 分别使用只读模式与正常完全开启模式,同时开启两个档案(Fig 9),复制只读模式文件设定并粘贴到正常完全开启模拟文件设定。在此演示两种场景,复制物理模型 (Fig 10-Fig 12),复制Reports (Fig 13-Fig 15)Graphical user interface, application  Description automatically generated
                                                    Fig 9
Graphical user interface, application  Description automatically generated
                                                      Fig 10
Graphical user interface, application  Description automatically generated
                                                      Fig 11

                                                  Fig 12
Graphical user interface, text, application  Description automatically generated
                                                                 Fig 13
Graphical user interface, text, application  Description automatically generated
                                                               Fig 14
Graphical user interface, text, application  Description automatically generated
                                                                  Fig 15

3. Summary:
(1) 本报告说明STAR-CCM+ Power session License如何使用只读模式 (Read-only Mode)功能。
(2) 演示3种场景应用,扩大客户端License的使用范围,对于模拟文件创建更快与减少错误。
 

知识库文章 ID# KB000048837_ZH_CN

内容

摘要详细信息

关联组件

Design Manager Electronics Cooling In-Cylinder (STAR-ICE) Job Manager Simcenter STAR-CCM+