Simcenter Testing Solutions Simcenter Testlab Impact Testing and Impact Post Processing

2022-09-27T16:09:25.000-0400
Simcenter Testlab

요약

It is described about a structural testing using hammer impact excitation. This testing is included from task documentation, channel setup and calibration, trigger setup, and selection of the optimal point of excitation to the actual measurement and further validation. And it also includes all the steps for offline use.


세부 정보


It is described about a structural testing using hammer impact excitation. This testing is included from task documentation, channel setup and calibration, trigger setup, and selection of the optimal point of excitation to the actual measurement and further validation. And it also includes all the steps for offline use.

KB 자료 ID# KB000065665_KO

내용

요약세부 정보

관련 구성 요소

Simcenter Testlab Digital Image Correlation Testlab Environmental Testlab Acoustics Testlab Data Management Testlab Desktop Testlab Durability Testlab General Acquisition Testlab General Processing & Reporting Testlab Rotating Machinery & Engine Testlab Sound Designer Testlab Structural Dynamics Testlab Turbine