In this tutorial, a simple simulation of a guitar string will be used to illustrate the process of performing a prestressed modal analysis in Simcenter 3D.
This tutorial is divided into 4 parts:
1. Introduction and equation for hand calculation
2. Guitar string Geometry creation and setup SIM and FEM files
3. Mesh and assign material properties to Guitar string
4. Apply boundary conditions, solve and postprocess the model
Please follow the previous parts of this tutorial here:
Pre-Stressed Modal Analysis of a Guitar String tutorial - Part 1/4 - BackgroundPre-Stressed Modal Analysis of a Guitar String tutorial - Part 2/4 - Guitar string Geometry creation and setup SIM and FEM filesPart 3: Mesh and assign material properties to Guitar stringStep 05: Create the Mesh
•Select the 1D Mesh

tool in the Mesh group of the Home tab tool ribbon
•Select the line
•Ensure that Type is set to CBEAM
•Set Mesh Density by to Size
•Set Element Size to 5mm
•Click OK
Step 06: Assign Materials and Properties
•Expand the 1D Collectors item in the Simulation Navigator
• Right-click on the Beam Collector(1) item and select Edit
•In the Mesh Collector menu that appears, click on Edit
•Click on the Show Section Manager

button for Fore Section
•In the Beam Section Manager menu select Create Section
•Ensure that the Beam Section is a ROD and enter 0.2413mm for DIM1
•Click OK and then Close
•Click on the Choose Material

button for Material
•Select AISI_Steel_4340 from the list that appears then click OK