NX2306シリーズでは、測定コマンドの「測定の設定ダイアログ」で、測定>ボディタブ>密度をチェックして、測定を実施しても、密度は「0.0」で表示されます。
NX2212シリーズでは、ソリッド密度は以下のように動作していました。
これはNX2306シリーズで発生している不具合で、NX2406で修正されます。
回避策は、以下の2つありどちらかをご利用ください。
1.設定で「情報ウィンドウに結果を表示」をONにする。
2.「ファイル>設定>ユーザインタフェース>ダイアログおよび精度>小数点未満桁数」を10に変更することで小数点表記で結果を表示できます。
これは表示の問題で正しく計算されていますが、NX2212シリーズのように浮動小数点表記になりません。
Related English version of the article : PL8751809