How to migrate Holes.txt file to the new Holes database format.

2021-10-06T23:50:58Z

Summary


Details

How do you convertthe old Holes.txt hole table to the new database style?



Solution

Hole database converter is used for legacy hole databases (holes.txt, 
threads.txt), and a holes database converter is provided. These two legacy 
databases are written to a new hole database file and are located in the 
../Program Files/Solid Edge ST10/Preferences/Holes folder. Solid Edge only 
recognizes the hole databases that are contained in this folder. 

Note: Make sure the decimal point symbol of the values in the text file 
matches the system decimal point. The values will be converted incorrectly if 
the symbols do not match


The Hole Database Converter is located in the C:\Program Files\Solid Edge 
ST10\Custom\HoleDatabaseConverter\bin directory. Once in there you can run the 
Hole Database Converter.exe and specify the text file to convert.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2012
Product: SOLID_EDGE
Application: APPLICATION
Version: V110.0
Function: SE_ADMIN

Ref: 001-8978145

KB Article ID# PL8978145

Contents

SummaryDetails

Associated Components