Drawing base view is missing components that show in modeling

2021-10-06T23:26:06Z

Summary


Details

When the user is placing the Base view on the drawing, it  is missing components.



Solution

In order to confirm which components should be shown on the drawing view, go to the Modeling application within the drawing file and use MB3 --> Replace View to show the view to be displayed as the base view on the drawing - all components that are displayed will show on the drawing.


Change application back to Drafting, select the Base View icon and look at the Part panel. Under Loaded Parts, ensure that the DRAWING file itself is the one selected and not any other file. This will use the view from the drawing and not from the master model part or any component.

Highlight the drawing file in the Base View dialog and then in the Model View panel, select the desired view from the  Model View to Use drop down menu and add the desired Base view -  now you will see all the expected components just as they were seen in Modeling.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: DRAFTING
Version: V10.0.3
Function: DRAWING/VIEW

Ref: 001-8977299

KB Article ID# PL8977299

Contents

SummaryDetails

Associated Components