Simcenter 3D Solutions Material orientation exists even though it has not been defined

2021-10-06T23:26:06Z
Simcenter 3D

Summary


Details

Material orientation (e.g. on shell elements like CTRIA or CQUAD) exists and

can be displayed,

even though user hasn't set anything related to it.

Solution

This is by design.

If we see inside the mesh associated data, we'll find that by default the

Material Orientation Method is set to "Orientation Angle". And since no value

has been set, zero will be used to determine the direction, which means it is

aligned with the x-axis.

This is in accordance e.g. with the CTRIA3 format definition from the online

help.

/>https://docs.plm.automation.siemens.com/tdoc/nx/11.0.2/nx_help/#uid:id489311

The definition of the method "orientation angle" can be found here:

/>https://docs.plm.automation.siemens.com/tdoc/nx/11.0.1/nx_help#uid:id629876

"Orientation Angle - Specify an angle. The software orients the X-axis of the

material coordinate system using the specified angle from the first edge of

the element."

The first edge of the element is referring to the edge that is constructed

from the first two nodes that are listed on NX-Nastran code. On NX, we can

display this using "Solver Syntax Preview":

Take for example this CTRIA3 element nr. 414:

$TRIA3 EID PID G1 G2 G3

CTRIA3 414 1 316 315 314

The vector that is formed from node 316 to node 315 defines the material

orientation for this tria element.

Notes

KB Article ID# PL8972529

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow