How to create Block of drawing view?

2021-10-06T23:50:56Z

Summary


Details

When we draft a view from part and retrieve a dimension and then try to create a block for the same. It is not possible. Is there any other possible way for the same.

Solution

You can create a block from drawing view by converting it to 2D drawing view. Below are the step.
 
Steps:
Step 1. Create a drawing of active model or start new draft file.
Step 2. Place desired drawing view in draft sheet.
Step 3. Select the placed drawing view > RMB (Right Mouse Button) Click > Select 'Convert to 2D View'.
Step 4. Select 2D view > RMB (Right Mouse Button) Click > Select 'Draw in View'.
Step 5. Select Block Command and > Select Geometry to add in Block > Select Block - Origin > Type name for Block .
Step 6. The created block can be placed using the Place Block command available from a block's shortcut menu in the Block Selection Pane. All of these methods allow you to set the scale and change the rotation of the graphics before they are placed.  

For more information about Blocks; please refer to Solid Edge Help for 'Using blocks'.  

Notes and References

8972463

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V109.0
Function: BLOCKS

Ref: 001-8972463

KB Article ID# PL8972463

Contents

SummaryDetails

Associated Components