ID balloon stub display - zero Stub Length vs. Without Stub

2021-10-06T23:26:06Z

Summary


Details

When creating or editing ID balloons, a user may want to eliminate the stub. There are two ways to do this and they have differing attachment results.



Solution

Without Stub results:
o Access the Balloon dialog 
o In the upper left corner of the dialog select the Option icon next to the 
   balloon dialog title 
o Select "Balloon (More)" to insure that all dialog options are displayed 
o Expand the Leader panel 
o Set Type = "Without Stub" 
   - Notice at this point that the Stub Side option is removed in the Style panel
o Create your balloon
   - The leader will now always be directed through the CENTER of the balloon regardless of the origin

Zero Length Stub:
o Access the Balloon dialog
o Set Type = "Plain"
o Stub Side = "Inferred" in Style panel
o Set Stub Length = 0.0
o Locating the ID balloon with these settings results in the leader attaching to either side of the balloon





Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: ANNOTATION

Ref: 001-8969360

KB Article ID# PL8969360

Contents

SummaryDetails

Associated Components