Showing CAM Notes in the PTP file

2021-10-06T23:26:06Z

Summary


Details

How can you add the operation note into the posted code file?

Solution

This information is located in the NX11 Help. 

The important part of this is that the mom variable mom_operation_notes will need to be used in the post to output the notes in the posted file.

Notes in Manufacturing

You can add multiple lines of informative text to any operation. 

The Notes dialog box is available as follows:

—All operation dialog boxes, in the Description group. 

—From the operation shortcut menu in the Operation Navigator . 

You can add the Notes column in the Operation Navigator by right-clicking in 

the navigator background and the selecting Column ?Notes . 

The icon indicates that there are notes stored with the operation. To display 

the note, pause your cursor on the icon. 

In the Notes dialog box, you can cut, paste, copy, insert text from a file, 

and save your notes as a text file. 

The mom variable mom_operation_notes outputs operation notes for post and shop 

documents. 

Where do I find it?

Application --> Manufacturing 

Command Finder --> Notes 

Operation Navigator --> Right-click an operation --> Notes 

 

Notes

KB Article ID# PL8969298

Contents

SummaryDetails

Associated Components