Space Reservation is Transparent when Editing the Path

2021-10-06T23:26:05Z

Summary


Details

Space Reservation is turning 50% translucent when editing the Space Reservation after the object display was edited to 0% translucency. 



Solution

The translucency goes back to 50% when it was set and saved at 0%.  This is because the default for the Space Reservation is 50%. The default can be changed to 0%.

In the Customer Defaults, there is a "space reservation stock translucency" setting, which by default is set to 50%.


Use the File -> Utilites -> Customer Defaults -> Routing, General, Stock tab, "Space Reservation Stock Translucency", and change the value to 0%. 



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2000_SP2
Product: NX
Application: ROUTING_GENERAL
Version: V11.0.2
Function: STOCK_AS_COMP

Ref: 001-8968522

KB Article ID# PL8968522

Contents

SummaryDetails

Associated Components