Controlling sketch dimension tolerance style display - tolerance is out of proportion to dimension

2021-10-06T23:26:05Z

Summary


Details

How to adjust the size of the tolerance display relative to the dimension when enabling sketch dimension display.

Solution

  • In the Part Navigator select the sketch and MB3 --> Show Dimensions to enable dimension display when   the sketch is not active.
  • Select a dimensions to add tolerance display and use MB3 --> Settings--> Tolerance --> Type --> and select display mode such as Bilateral Tolerance.
  • While still in Settings dialog expand Text--> Tolerance Text  and UNCHECK Scope --> Apply to Entire Dimension and under Format --> Height and decrease the value to get the optimal display.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: DESIGN
Version: V9.0.3
Function: SKETCHER

Ref: 001-8967509

KB Article ID# PL8967509

Contents

SummaryDetails

Associated Components