No value is being reported for 'Weight' in the Assembly Navigator

2021-10-06T23:26:05Z

Summary


Details

A material has been assigned to the model, but the weight value is not appearing in the 'Weight' column in the Assembly Navigator.



Solution

This is due to the weight data not being updated. This can be updated in the Part Properties dialog by 
enabling the option to update on save, or it can also be manually updated. 

Here's how to update the weight in the Assembly Navigator:
  1. In the Assembly Navigator, highlight the component that requires the weight to be updated.
  2. MouseButton3-->Properties.
  3. Select the 'Weight' tab.
  4. Here, the option to 'Update Data on Save' can be enabled so the weight is automatically updated upon a Save operation.
    Or the 'Update Weight Data Now' icon (270 degree arrow icon) can be selected to update the data immediately.

Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V10.0
Function: ASSEMBLY_MODEL

Ref: 001-8966652

KB Article ID# PL8966652

Contents

SummaryDetails

Associated Components