Specific Note - Terminating Object

2021-10-06T23:26:05Z

Summary


Details

How to Assign a Leader to a Region or an Entire Body when using Modeling PMI. 



Solution

Here is a list of note functions that allow users to select a Solid Body, as the "Associated Objects".  The list includes; Note (annotation group), General Note (specialized group), Coordinate Note, Enterprise Identification, Material Specification, Part Identification, Process Specification, URL Note, Locator 
Designator, String Note, Number Note, and Integer Note.


When assigning the leader, make sure the Selection Dialog has the "Point on Face" option selected, so that the user can select any face.  The leader itself cannot be assigned to a Solid Body, but the PMI can be associated to a Solid Body, as there is no "region" to select, only the faces of the body. 



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2008_R2
Product: NX
Application: PMI
Version: V11.0.1
Function: ASSOC_OBJECT

Ref: 001-8965598

KB Article ID# PL8965598

Contents

SummaryDetails

Associated Components