Simcenter 3D Solutions Plane Strain elements in FEM 2D axisymmetri does not export out the pressures

2021-10-06T23:26:04Z
Simcenter 3D

Summary


Details

If plane strain or plain stress element types are used in a Nastran 2D Axisymmetry FEM file, the later versions of Advanced Simulation or Simcenter Pre-Post, uses different load types for pressure. 

Solution

Plane Stress and Plane Strain elements, such as CPLSTS4 and CPLSTN4 elements, use the PLOADE1 load for edge loads as surface tractions. PLOADX1 is the pressure load for axisymmetric elements, such as CQUADX4 CTRIAX6 elements. 

The Nastran 2D axisymmetric solver User Interface, in NX 9 and 10, uses the edge load function that creates PLOADE1 card. The Pressure load function exports out the PLOADX1 load cards for axisymmetric elements. .

NX/Simcenter Pre-Post 11, User Interface combines both functions into the Pressure Load function. The card name on the pressure dialog lists the card types as PLOADX1/PLOADE1. If the elements are of the type Plane Stress or Plane Strain, PLOADE1 cards will be creates. If the element types are Axisymmetric, such as CTRIAX6 and CQUADX4, the PLOADX1 cards will be created instead.

Notes

KB Article ID# PL8965329

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow