Simcenter 3D Solutions Using Thermal/Flow, but Sometimes the Element IDs/Labels Don't Match in Post Processing.

2021-10-06T23:26:05Z
Simcenter 3D

Summary


Details

Assume we are using NX Thermal/Flow, Electronic Systems Cooling or Space Systems Thermal.  Sometimes it seems when doing Post Processing there's additional elements that have been created.  For example the .FEM model includes only 3D solid elements but in post processing there's also 2D elements.  Furthermore in the MSGF file there's a message as follows:

Note: During the analysis process a number of elements have been created whose labels you may not recognize. To find out more about  these elements and the elements they are associated with, please  look on file REPF for the phrase 'TMG element'.

What is the explanation for this behavior?

Solution

For boundary conditions the 3D solid elements need to be surface coated with 2D elements.  If the surface is not manually coated by 2D null shell elements in the .FEM then the solver creates these elements on the fly.  Hence the model element IDs/labels don't correspond with those in post processing.  It is recommended to coat the surfaces on which the boundary conditions are applied to ensure that the element IDs reported by the model and post processing are the same.

Notes

IR 8965232.

KB Article ID# PL8965232

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow