Wave Linked PMI becomes retained

2021-10-06T23:26:06Z

Summary


Details

Loading assembly using Latest Working load options will cause linked PMI to 
become retained when component is revised in Teamcenter


(1) Create the following assembly:


Assembly 
 |-- Component


(2) In Component file, create a PMI on the geometry 
(3) Use Linked PMI to link the component PMI to the assembly 
(4) Save and Close all data in NX 
(5) In Teamcenter, revise the component to next new revision 
(6) Load the assembly with Latest Working load option. 
Notice the linked PMI becomes retained.


How to fix this retained linked PMI? 



Solution

When the linked PMI is retained, use the Replace Component operation in
Assembly Navigator to replace the component with the previous revision,
the one that the linked PMI was originally created from. Now the linked PMI 
should become up to date.
In Assembly Navigator, use Replace Component operation again to replace the 
component back to current desired revision. That linked PMI will remain up to 
date.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: PMI
Version: V9.0.3
Function: WAVE

Ref: 001-8964352

KB Article ID# PL8964352

Contents

SummaryDetails

Associated Components