Geometry is not visible or selectable in a part Modeling Application

2021-10-06T23:26:06Z

Summary


Details

Have you ever experienced a strange behavior in your part where you are unable to see curves after using certain command like Stretch Curve or select the edge or end point at a particular location of your part?
NX behaves like there is a clipping plane at a particular corner of the part.



Solution

The problem could cause by Section Clipping Plane.


You can try either 2 options below to fix the problem:


1) Toggle Off the "Clip Section" button which is located in the View ribbon or Menu --> View --> Section --> Clip Section.

Or:

2) Launch "Edit Section" from the 2 locations mentioned above and move the current clipping plane to a new distance either dragging the vector or enter a new distance in the dialog.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V9.0.3
Function: DISPLAY

Ref: 001-8947775

KB Article ID# PL8947775

Contents

SummaryDetails

Associated Components