LOV's value not coming through for custom attributes

2021-10-07T00:01:12Z

Summary


Details

A custom attribute 'Robot_Manufacturer' is defined under Robot class. On this 'Robot_Manufacturer', the customer defined a list of values with 5 values. When they checked it in the Process Designer, the LOV list is not populating. Under ListOfValues.xml the entry is there for it. <EnumerationField FieldName="Robot_Manufacturer" ClassName="Robot"> Also, they tried on 'supplier' property, which is on 'ToolPrototype' and on that also it is not populating the LOV.

Solution

This issue is Works As Designed, and the recommended practice for visualizing eMS custom LOVs in Process Designer is Table View. In Table View, or (TV) the application utilizes the system root LOV.xml file in conjunction with the database numerical value to display the nice name. In the Properties Viewer we display only the database value (ie 01, 02). In TV, it is recommended to create custom configurations for the different resource library types. This will allow for visualizing the attributes and all like resource types in one view, and not picking through each type individually.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANNING_APPLIC
Version: V13.1
Function: PROCESS_DESIGNE

Ref: 001-8935956

KB Article ID# PL8935956

Contents

SummaryDetails

Associated Components