NX Importing a drawing assembly into Teamcenter raises an Attribute Validation Error

NX for Design

Summary


Details

Importing a drawing assembly into Teamcenter raises an Attribute Validation Error on "OWNING_GROUP"

The NX syslog records the following error;

      Attribute Validation Error : The value being set is not contained in the list of values.       For Logical Object: #######-001.prt, Title : OWNING_GROUP

Solution

Open the part in Native NX and check the Properties for the property noted as the "Title:", in this example, "OWNING_GROUP". If the value for that property is removed or if the property is deleted, then saving the part(s) , the assembly can then be imported into Teamcenter without error.

KB Article ID# PL8829905

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX