No Custom Symbols found in the Reuse Library after upgrading NX.
SolutionFrom NX 2306, you can do the custom symbol installation from inside NX the command is located as below:
The reference documentation is as the link below (just need to select “Custom Symbol” in first step):
https://docs.sw.siemens.com/en-US/doc/209349590/PL20221117716122093.reuselib/xid2213814
After importing the symbols into TC, please check these two things:
Add the location of imported symbol library in Reuse Library, one method is to change the customer defaults setting as above; another method is to use command dialog “Library Management” from Reuse Library navigator, the steps are:
a) Select category “Custom Symbol Library”.
b) Click the button “Add Library” and select the folder of imported symbols.
NOTE - installation is not required for symbols in native environment, just unzip the symbols in a native folder, and add that folder as a library (same steps as above).