How to export dxf, dwg, step, iges files to other dataset types/custom datasets, from the default image datasets in Teamcenter, using the NX translator.
SolutionYou can use the "TC_NX_DataExchange_Dataset_Preferences" Teamcenter user preference to define or edit the dataset properties used by NX translators to import from and export to Teamcenter.
Each line must specify a translator and its workflow, extension, dataset type, dataset relation, and named reference type.
The syntax of each translator-specific line should be as follows:
The parameters used in the syntax are defined as follows:
Please refer to the below documentation.
https://docs.sw.siemens.com/en-US/doc/209349590/PL20231101866122454.dataexchange/xid1676860?audience=external&pk_vid=bc87182906d9eb7d81eb1f21a59b0ef51721031302e7971c