Unable to get Solid Edge option/icon in Import Parts for 2D Nesting

2024-12-31T04:47:10Z

Summary


Details

Unable to get Solid Edge option/icon in Import Parts for 2D Nesting

Solution

Navigate to "C:\Program Files\Siemens\Solid Edge 2D Nesting 2025\Preferences" (or the folder where 2D Nesting is installed).

In the Preferences folder, locate the settings.ini file and open it with Notepad.Check if the 'SolidEdgeSupport' option is present and set to True

SolidEdgeSupport = True

If the line is missing, add it and set it to True so that the Solid Edge icon appears in the Import Parts section.

KB Article ID# PL8824804

Contents

SummaryDetails

Associated Components