In Drafting the Flat Solid is not displayed in all the views [TOP, Bottom, etc.]]

2024-12-30T17:52:15Z

Summary


Details

In the drafting application, the flat solid view is not visible in the drawing view, even though all the layers are visible, and the flat solid view is displayed at the assembly level in system-generated views.

Solution

The current behavior is as designed.

Before NX2306 the Flat Solid View was not available so the Flat Solid is displayed in all the views [TOP, Bottom, etc.] 

From NX2306 we created a new view for each Flat Solid feature made in the Sheet Metal application.


This new view has the below behavior.

1. Flat solid objects are visible in all model views(Top, bottom, etc.), but only flat solid objects/bodies are visible in the Flat Solid model view.

2. In drafting the "Base View" dialog, a flat solid view is listed and if the user places the Flat Solid drafting view curves are created for the bodies and components that are available in the Flat Solid model view. Then using the layer settings the user should control the visibility of components in the Drafting Flat Solid view.

3. When the user imports system generated views (Top, bottom etc.) in the drawing the sheet Flat Solid objects can't be visible in those views in drafting.

Notes

11170657

KB Article ID# PL8824220

Contents

SummaryDetails

Associated Components