I want to check and operate invisible edges

2024-12-09T23:10:03Z

Summary


Details

If the rendering style is shading or hidden lines, it is not possible to understand hidden edges. For example, in the case of Sketch feature, is there any way to check this? Also, is it possible to input blends, etc. to the hidden edges?


Reproduced Steps:
1. Create a Sketch and extrude it




2. Create a Block feature on top of the extruded feature( with Unite)



When selecting sketch geometries, only the visible sketch lines are highlighted.


Solution

“Selection” group – “Highlight Hidden Edges”
Highlight a hidden edges by selecting an edge in the model or a feature in the part navigator.




“Selection” group – “Allow Selection of Hidden Edges”
Hidden edges can be selected while performing various commands (for example, Edge Blend).



Notes

**Please refer to PL8822608 for Japanese article.

Release Versions
  • NX V2306
  • NX - DESIGN V2306
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8822609

Contents

SummaryDetails

Associated Components