Made Human model and when opening Assembly the Human fails to display

2024-12-16T21:56:21Z

Summary


Details

Made Human model and when opening assembly the Human fails to display

Solution

Users may not realize the Human model is created from Facets, which is a Lightweight Body, and is not a Solid or Sheet body.

Only Solid or Sheet bodies are automatically added to the default Reference Set, which is configured within Customer Defaults.

Adding the Human to the company's default Reference Set within the part file it resides within, now allows the Human to display in the assembly when opened as expected.


KB Article ID# PL8822311

Contents

SummaryDetails

Associated Components