Place a driving dimension to a theoretical intersection

2025-03-12T17:05:00Z

Summary


Details

In Solid Edge 2024, it is possible to place a "driven dimension" in a sketch using the "distance between" function between theoretical intersections, as shown below.


However, it is not possible to turn this into a "driving dimension" (a red dimension).

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V224UPD10
Solution

Placing a "driving dimension" with the "distance between" function, between theoretical intersections is possible in Solid Edge 2025.

Notes

KB Article ID# PL8820231

Contents

SummaryDetails

Associated Components