End of Maintenance for Solid Edge X (v2410) suite of product is listed below. These dates represents when Siemens Digital Industries Software will discontinue providing ongoing maintenance releases, along with the last Teamcenter release supported. After these dates, no further maintenance releases will be issued for the corresponding Solid Edge version.
SolutionSolid Edge X (v2410):
Solid Edge X (v2410) End of Maintenance (EoM): 31st January 2026
Solid Edge X (v2410) Extended Support until: 31st July 2026
Mainstream Support is 15 month of Update support from the Release to Manufacturing (RTM) Date. Extended Support is End of Maintenance (EoM) plus 6 month for select critical fixes with additional Updates, as required.
Solid Edge X & Teamcenter Integration
Solid Edge X (v2410) Essentials
Solid Edge X (v2410) Premium
Click here and follow the information to review the detailed, actual "End of Maintenance dates for Teamcenter Integrations" (Solid Edge & Teamcenter Integration EoM SFB v301024.pdf) Information.
NotesIf you are looking for another Solid Edge Version End of Maintenance Information, go to Solid Edge and Solid Edge X Version End of Maintenance Information (Collection)
Support Information
PLMS will continue to provide support and assistance for Solid Edge. PLMS will attempt to duplicate any possible code defects on the revision of software in which the defect is reported (when available) and on the current release or Update of the product. PLMS will not create a PR unless the problem can be duplicated in a supported version of the product. If it is found that the defect does not occur in the latest revision of the software, the customer will be asked to update their product to the current revision to correct the problem.