Tecnomatix Controllers for ABB_RAPID, ABB_RAPID_VOLVO, DUERR_ECOTALK, FANUC_RJ, FANUC_RJ_JAPAN, FANUC_RJ_VOLVO

2024-11-18T05:44:45Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "ABB_RAPID, ABB_RAPID_VOLVO, DUERR_ECOTALK, FANUC_RJ, FANUC_RJ_JAPAN, FANUC_RJ_VOLVO"
are available for download from https://support.sw.siemens.com.

See Tecnomatix__changes_log.html for details concerning this update.
Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix Robot Controllers' folder.


Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select Tecnomatix 17.0, 2206, 2301, 2307, 2402 or 2408
-Select Tecnomatix 17.0 Robot Controllers, Tecnomatix 2206 Robot Controllers, Tecnomatix 2301 Robot Controllers, Tecnomatix 2307 Robot Controllers, Tecnomatix 2402 Robot Controllers or Tecnomatix 2408 Robot Controllers
[Or Select 'Additional Downloads' / 'Older Versions' to access 16.1, 16.1.1 or 16.1.2]

Download the file(s):

Tecnomatix_16.1_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_16.1_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_16.1_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_16.1_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_16.1_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe

Tecnomatix_16.1.1_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_16.1.1_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_16.1.1_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_16.1.1_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_16.1.1_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe

Tecnomatix_16.1.2_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_16.1.2_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_16.1.2_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_16.1.2_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_16.1.2_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe

Tecnomatix_17.0_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_17.0_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_17.0_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_17.0_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_17.0_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe

Tecnomatix_2206_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_2206_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_2206_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_2206_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_2206_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe
Tecnomatix_2206_FANUC_RJ_VOLVO_64BIT_v1.3_15_11_2024.exe

Tecnomatix_2301_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_2301_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_2301_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_2301_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_2301_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe
Tecnomatix_2301_FANUC_RJ_VOLVO_64BIT_v1.3_15_11_2024.exe

Tecnomatix_2307_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_2307_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_2307_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_2307_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_2307_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe
Tecnomatix_2307_FANUC_RJ_VOLVO_64BIT_v1.3_15_11_2024.exe

Tecnomatix_2402_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_2402_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_2402_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_2402_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_2402_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe
Tecnomatix_2402_FANUC_RJ_VOLVO_64BIT_v1.3_15_11_2024.exe

Tecnomatix_2408_ABB_RAPID_64BIT_v5.34_15_11_2024.exe
Tecnomatix_2408_ABB_RAPID_VOLVO_64BIT_v5.23_15_11_2024.exe
Tecnomatix_2408_DUERR_ECOTALK_64BIT_v3.7_15_11_2024.exe
Tecnomatix_2408_FANUC_RJ_64BIT_v5.11_15_11_2024.exe
Tecnomatix_2408_FANUC_RJ_JAPAN_64BIT_v3.10_15_11_2024.exe
Tecnomatix_2408_FANUC_RJ_VOLVO_64BIT_v1.3_15_11_2024.exe



To Install:

Place Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.


If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8819923

Contents

SummaryDetails

Associated Components