It is possible to store NX post processors in Teamcenter so all users are served the same posts on demand. How to set this up?
SolutionPlease see the attached "How to import posts into Teamcenter".
document on this process. Essentially, the posts come in to a dedicated folder in TC via an import script. If there are existing classified machines already in TC, the posts will be associated to the proper machine and be loaded as the default post when that machine is imported to the setup. If they are just standalone posts, they will simply live in TC for the user to select as needed.
Also, please reference the attached "Importing NX CAM setup into TC.pdf" file for information on importing custom simulation machines and cam setups into TC as part of the prerequisites for importing the post processors.
Notes