Yaskawa Motoman RCS not initializing

2024-11-11T20:11:14Z

Summary


Details

Yaskawa Motoman RCS not initializing

Solution

When working with Yaskawa robots there is a mandatory step to create the .ctl file. To create the .ctl file,

go into Robot > Setup > Robot Properties > External Axes Setup at least once, so that the .ctl is created under the machine data files folder.


Notes

Not sure why the RCS needs this file when there are no external axes, but that's the way the Yaskawa RCS works.

KB Article ID# PL8819045

Contents

SummaryDetails

Associated Components