The displayed values of Radius Analysis results are opposite for "Minimum" and "Maximum"

2024-11-05T23:40:14Z

Summary


Details

When checking the analysis result on the dialog, the minimum value is large and the maximum value is small, but I think this is the opposite.

Solution

This behavior is working as designed.
The numbers shown on the dialog are not radius but curvature radius. So "Minimum" represents the minimum curvature radius and "Maximum" represents the maximum curvature radius.

1. Analysis tab > Face Shape group > More > Radius 


Notes

**Please refer to PL8818347 for Japanese article.

Release Versions
  • NX V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8818352

Contents

SummaryDetails

Associated Components