SEEC: Need to use SEEC Dispatcher to create PDF's

2024-10-30T11:26:06Z

Summary


Details

When running the SEECDispatcher.exe a Validation Successful message is returned but nothing else happens. Is the SEECDispatcher.exe working correctly?

Platforms
  • INTEL windows-1064
Release Versions
  • Solid Edge V223.0
Solution

When running the SEECDispatcher.exe the Teamcenter credentials are validated. When "Validation Successful" appears the process is complete.

Notes

KB Article ID# PL8817532

Contents

SummaryDetails

Associated Components