Bundle changes wire path definition

2024-10-14T12:11:50Z

Summary


Details

When a bundle is created the paths of the wires are altered. For example, a wire path is routed through a component. When the bundle is created the wire path regenerates and is no longer routed through that component.



Solution

Creating a bundle splits the wires, which causes the behavior.

Use the Route command after creating a bundle.



Release Versions
  • Solid Edge V224.0
Platforms
  • Windows x64 11
Notes

KB Article ID# PL8815444

Contents

SummaryDetails

Associated Components