Hide Sketch XY Axis

2024-10-10T21:24:08Z

Summary


Details

I can hide the sketch axis by "Invert Shown and Hidden", but other sketch objects are also hidden. Is there a setting to hide only the XY axis of the sketch?
Reproduced Steps:
1. Enter Sketch



2. Menu > Edit > Show and Hide > Invert Shown and Hide


Solution

There is no function to control Show/Hide of sketch axes and origin.
Additionally, the phenomenon where the sketch axis becomes invisible when using "Invert Shown and Hidden" is due to a bug in NX, and will be fixed in NX 2412 so that it will not become invisible.

Notes

**Please refer to PL8814891 for Japanese article.

Release Versions
  • NX V2406
  • NX - DESIGN V2406
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8814893

Contents

SummaryDetails

Associated Components