Command line to silently uninstall Solid Edge 2024 Update 9

2024-11-12T11:42:27Z

Summary


Details

What is the command line to silently uninstall Solid Edge 2024 Update 9?

Solution

The command line for Solid Edge 2024 Update 9 (build 224.00.09.004) is:

msiexec /package {FAF68E69-27BE-4111-A3EF-245C40A1C7F2} /uninstall {505E699F-E2BC-49B3-8D88-6CE9B2293EFD} /qn+ /norestart /log C:\temp\2240009004_uninstall.log

Notes

To the parent article

KB Article ID# PL8814868

Contents

SummaryDetails

Associated Components