Change the angle of the Detail View

2024-10-10T01:24:24Z

Summary


Details

Is there a way to create a detail view so that a slot shape is horizontal to the drawing?

Reproduced Steps:
1. Preparation of model with a slot shape
2. Creating a base and a detail views in the drawing


Solution

When creating a detail view from a base view, you cannot control the placement angle (for example, to make the slot shape horizontal). However, after creating the detail view, you can change it to an independent detail view and specify the placement angle so that the slot shape is placed horizontally in the drawing.

1. Select Detail View > Mouse light click > Convert to Independent Detail


2. Select Detail View > Mouth light click > Settings > Common > Angle


Result


Notes

In addition when specifying "Angle", you can specify "Associative" so that it will automatically follow if the angle of the slot shape changes. For example, when creating a slot shape in a sketch, you can have the angle of the slot relative to the horizontal as a parameter and make use of a formula when specifying "Angle".




**Please refer to PL8814761for Japanese article.

Release Versions
  • NX V2212
  • NX - DRAFTING V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8814763

Contents

SummaryDetails

Associated Components