Column Width and Row Height of PMI Table are not inherited to drawings

2024-10-09T23:57:04Z

Summary


Details

When I inherit a PMI table and place a view on a drawing, Column Width and Row Height change. As a result, text may overflow the cell or be split into two lines. Is it possible to inherit the table Column Width and Row Height in the same way?

Reproduced Steps:
1. Insert a PMI Table



2. Create a view in Drawing Sheet(Inherit PMI to drawing view )


Solution

This behavior is working as designed, and is entered using the table column width and row height set in the drawing environment.
However, by using "Inherit PMI Tracking", you can inherit various PMI table settings.
1. In Drafting, Menu > Format > PMI > Inherit PMI Tracking

2. Turn TableColumnWidth and TableRowHeight ON

    TableColumnWidth:Table Column Width
    TableRowHeight : Table Row Height



Notes

**Please refer to PL8814481 for Japanese article.

Release Versions
  • NX V2212.5000
  • NX - DRAFTING V2212.5000
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8814759

Contents

SummaryDetails

Associated Components