"Wireframe with Dim Edges" does not exist

2024-10-09T23:55:01Z

Summary


Details

In NX 2312, when displaying View Radial shortcut, "Wireframe with Dim Edges" did not exist and was replaced with "Wireframe".
When applying this rendering style, the hidden edges were not visible, but is it possible to make them visible?

View Radial shortcut that was displayed before NX 2306:




Reproduced Steps:
1. Mouse right click in the graphics window > “Wireframe”


Solution

With the enhancements in NX 2312, the following three rendering styles have been unified into "Wireframe":
- Wireframe with Dim Edges
- Wireframe with Hidden Edges
- Static Wireframe
You can switch between these by changing the "Visualization Preferences". To set the rendering style to "Wireframe with Dim Edges", set "File" > "Settings" > "Visualization" > "Rendering" > "Display" > "Wireframe Display Type" to "Dynamic".


Notes

What's new in NX 2312 : Wireframe display


https://docs.sw.siemens.com/en-US/doc/209349590/PL20230425446868577.whatsnew/xid2251065?pk_vid=342d656516f4836c42ba6d8985c43b481725401552870595
 for Japanese article.

**Please refer to PL8814479 for Japanese article.

Release Versions
  • NX V2312
  • NX - GATEWAY V2312
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8814480

Contents

SummaryDetails

Associated Components