It is not possible to return a borrowed license file earlier to the license server using the Siemens Licensing Tool.
A message comes up:
Failed to return licenses. Error:-63
This issue happened in SLS3.2.0 and 4.0.0.
It does not happened in SLS2.4.0.
This is a known issue.
The license server does not allow early return of borrowed features, the client will see a -63 error and the server will say the early return is not authorized. This will be fixed in a coming server release.
SolutionIf there is a need to give the license back, a reset can be done by a clear borrow license file.
Customer needs to ask for it in a ticket created in Support Center and it will be shipped out.