Precision Option for Decimal Control in Note Editor

2024-11-03T20:39:52Z

Summary


Details

Precision Option for Decimal Control in Note Editor.

Solution

Please see NX demonstration video above along with detailed instructions below.

The Precision option can be used to control the number of decimal places displayed in a note for object and part attributes as well as expressions.

Existing Note Instructions

1.  To use the Precision option on an existing note, right mouse button click on the note and select Edit.

2.  Place your cursor over the attribute or expression and right mouse button click to find the Precision option in the drop-down menu.  Click on the desired number of decimals to display for your value.

On Note Creation

1.  After you have inserted your attribute or expression into the note, right mouse button click to find the Precision option in the drop-down menu.  Click on the desired number of decimals to display for your value.

Notes

Please also refer to the What's New in NX 2406 documentation link below on Precision in object and part attributes.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20231101866122454.whatsnew/xid2287466

KB Article ID# PL8813814

Contents

SummaryDetails

Associated Components