No Hole Callout feature count with mixed hole types

2024-10-08T16:47:44Z

Summary


Details

A Drafting Hole Callout does not display the feature count when creating a callout that includes Pattern Features with different hole types

Platforms
  • All Windows N/A
Release Versions
  • NX V2406
Solution

NX Drafting Hole Callouts cannot display the feature count when a hole is included in a Pattern Feature in modeling that includes different hole types.

To overcome this limitation, the user must edit the Pattern Feature to only include a single hole type for each type. Once this is done the feature count can be included in the Drafting Hole Callout if desired and the correct count will be displayed.

Notes

KB Article ID# PL8812946

Contents

SummaryDetails

Associated Components