User case where attempting to create new component in an assembly and getting the error that the templates part is not available in Teamcenter.
NX is using the PAX files that are located in the Startup folder defined by the UGII_COUNTRY_TEMPLATES environment variable. UGII_COUNTRY_TEMPLATES=C:\Eng\NX####\localization\english
UGII_TEMPLATE_DIR=C:\Eng\NX####\UGII\templates
NX is using the PAX files that are located in the Startup folder defined by the UGII_COUNTRY_TEMPLATES variable.
Either the PAX files are not in the define location or they are not pointing to the correct parts in Teamcenter. The syslog records that the files are not found in the database;
Processing C:\Eng\NX####\localization\english\startup\nxdm_ugs_model_templates.pax for File New Templates
template specified by name @DB/model-plain-1-inch-template/A not found in database
To fix this, either disable or delete the UGII_COUNTY_TEMPLATES variable and restart NX