This FAQ is intended to provide an overview of relevant existing FAQs related to using Solid Edge and working with STEP data, sorted by categories "General", "Utilities & Resources", and "Troubleshooting".
This is a living document, which means that new FAQs and categories may be added to this collection.
Best Practices for Working with Imported CAD Data
Improving STEP file import performance in Solid Edge
Is there a way to batch convert Solid Edge documents to neutral format such as STEP?
Availability of the "Optimize" Command After Modifying Imported STEP Files
Free STEP File Analyzer and Viewer (will open a third-party resource)
STEP Standard - ISO 10303 (will open a third-party resource)
Utility for Automatic Optimization of Imported CAD Models in Solid Edge
STEP file opens but no geometry imported
Multiple Bodies Appear in AP242 STEP File Export
Exported STEP File Thread Color Issue
Solid Edge Fails to Import STEP File with No Visible Geometry