Tecnomatix Controllers for FANUC_RJ, FANUC_RJ_JAPAN, SIASUN_SNRC

2024-09-19T04:43:14Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "FANUC_RJ, FANUC_RJ_JAPAN, SIASUN_SNRC"

  are available for download from https://support.sw.siemens.com.

   See Tecnomatix_<ControllerName>_changes_log.html for details concerning this update.

   Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix <Version> Robot Controllers' folder.

Use the following steps to download:

- Login to https://support.sw.siemens.com

- If you do not have an account, click 'Register Now' and fill out the information.

- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.

   - Scroll down and toggle On the Tecnomatix product.

   - Scroll back to the top and click Support Center in the breadcrumb.

- Select 'Tecnomatix' from 'My Products'

- Select 'Download'

- Select Tecnomatix 17.0, 2206, 2301, 2307, 2402 or 2408

 -Select Tecnomatix 17.0 Robot Controllers, Tecnomatix 2206 Robot Controllers, Tecnomatix 2301 Robot Controllers, Tecnomatix 2307 Robot Controllers, Tecnomatix 2402 Robot Controllers or Tecnomatix 2408 Robot Controllers

  [Or Select 'Additional Downloads' / 'Older Versions' to access 16.1, 16.1.1 or 16.1.2]

Download the file(s):

    Tecnomatix_16.1_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_16.1_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_16.1_SIASUN_SNRC_64BIT_v1.17.1_18_09_2024.exe

    Tecnomatix_16.1.1_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_16.1.1_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_16.1.2_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_16.1.2_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_17.0_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_17.0_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_2206_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_2206_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_2301_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_2301_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_2301_SIASUN_SNRC_64BIT_v1.17.1_18_09_2024.exe

    Tecnomatix_2307_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_2307_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_2307_SIASUN_SNRC_64BIT_v1.17.1_18_09_2024.exe

    Tecnomatix_2402_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_2402_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_2402_SIASUN_SNRC_64BIT_v1.17.1_18_09_2024.exe

    Tecnomatix_2408_FANUC_RJ_64BIT_v5.7.1_18_09_2024.exe

    Tecnomatix_2408_FANUC_RJ_JAPAN_64BIT_v3.6.1_18_09_2024.exe

    Tecnomatix_2408_SIASUN_SNRC_64BIT_v1.17.1_18_09_2024.exe

To Install:

Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.

If you have any issues with the installation or support of these fixes,

please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8811893

Contents

SummaryDetails

Associated Components