NX Convergent Body Facet Edges displaying when turned off in Preferences?

2024-09-10T13:19:41Z
NX for Design

Summary


Details

Convergent Body Facet Edges displaying when turned off in Preferences?

Solution

Convergent bodies are created form multiple patches of surfaces and unlike conventional solid bodies, the edges can now be turned off. If you are using NX2406 or later, the Dim Edges option for Convergent Bodies is on by default so open  'File -> Preferences -> Visualization (preferences)' and uncheck the box called Display with Dim Face Edges..



KB Article ID# PL8810258

Contents

SummaryDetails

Associated Components

Modeling