Angular dimension appears to be incorrect when the round off is higher than 4 decimal places

2024-09-06T12:29:25Z

Summary


Details

Placed an angular dimension in a part profile that reads as 90.0000 degrees when the round off is set to 4 decimal places. When the round off is changed to 7 decimal places it reads as 89.9999800 degrees. How do you make it read as 90.0000000?

Solution

The default accuracy built into Solid Edge is set to .99 in the part's physical properties. Changing from .99 to 1 will make the dimension read correctly out to 7 decimal places with a +0/-0 tolerance. However, there may be a performance impact with this tight of a tolerance, depending on the complexity of the part geometry.

KB Article ID# PL8809773

Contents

SummaryDetails

Associated Components