Tecnomatix What Manus tracking gloves are supported?

2024-09-05T16:42:19Z
Virtual Reality

Summary


Details

What exact Manus tracking gloves are supported?

Platforms
  • na windows-1032
Release Versions
  • Tecnomatix V2402
Solution

"Quantum MoCap Metagloves" are supported in version Tecnomatix 2408.

From this version on, it is possible to use the gloves to interact with objects in the VR Sequencer. This is only enabled for the Manus glove today.

The "Data Glove" option shown in the Live Hands UI is only for the Synertial glove integration. This glove doesn't support interacting with objects in the VR Sequencer mode.

Notes

KB Article ID# PL8809315

Contents

SummaryDetails

Associated Components

VR Analyze